< Assembler Command Options / Microcontroller Options >
[Format]
The default for this option is endian=little.
[Description]
- | When endian=big is specified, data bytes are arranged in big endian.
When endian=little is specified, data bytes are arranged in little endian. |