< Assembler Command Options / Microcontroller Options >
This option outputs to the relocatable file the information about the general register that is specified to be used only as a base address register through the same-name option in the compiler. |
Be sure to set this option to the same value for all assembly processes in the project. If a different setting is made, correct operation is not guaranteed. |
Do not use a general register specified by this option for other purposes than a base address register. If such a register is used for any other purpose, correct operation is not guaranteed. |