< Optimizing Linkage Editor (rlink) Options / Options Other Than Above >
[Format]
[Description]
- | Specifies the end of the option specifications. |
- | This option cannot be specified on the command line. |
[Examples]
- | Command line specification: |
rlink -sub=test.sub -nodebug
|
input=a.obj,b.obj ; Processing (1)
start=P,C,D/100,B/8000 ; Processing (2)
output=a.abs ; Processing (3)
exit
|
- | Executes the processing from (1) to (3) and outputs a.abs. |
- | The nodebug option specified on the command line after exit is executed is ignored. |