< Library Generator Options / Library Options >
This option creates simple I/O functions that do not support the conversion of floating-point numbers (%f, %e, %E, %g, %G). |
When inputting or outputting files that do not require the conversion of floating-point numbers, ROM can be saved. |
Target functions: fprintf, fscanf, printf, scanf, sprintf, sscanf, vfprintf, vprintf, and vsprintf