Realtime OS Resource Information panel

This panel displays the resource information (e.g. system information and memory area information) of the RI850V4.

Figure A-1. Realtime OS Resource Information Panel



The following items are explained here.

- [How to open]

- [Description of each area]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Tab selection area

Select a tab to switch the content displayed in the Information display area.

This panel has the following tabs:

- [System] tab

- [Memory Area] tab

- [Task] tab

- [Semaphore] tab

- [Eventflag] tab

- [Data Queue] tab

- [Mailbox] tab

- [Mutex] tab

- [Fixed-Sized Memory Pool] tab

- [Variable-Sized Memory Pool] tab

- [Cyclic Handler] tab

- [Interrupt Handler] tab

- [Initialize Routine] tab

- [Extended Service Call Routine] tab

- [Ready Queue] tab

- [Timer Queue] tab

(2) Information display area

This area displays the resource information (e.g. system information and memory area information) of the RI850V4.