[Cyclic Handler] tab

This tab displays the cyclic handler information (e.g. Cyclic Handler Name and ID) of the RI850V4.

Figure A-23. [Cyclic Handler] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

This area displays the cyclic handler information (e.g. Cyclic Handler Name and ID) of the RI850V4.

This area consists of the following items.

Cyclic Handler Name

An icon indicating the current status of the cyclic handler and the name of the cyclic handler are shown in the following format.

Icon Name

Note that if the name of the cyclic handler is undefined, the name will appear as "ID".

Non-operational state (STP state)

Operational state (STA state)

ID

The ID of the cyclic handler is shown.

Status

The current status of the cyclic handler is shown.

TCYC_STP

Non-operational state (STP state)

TCYC_STA

Operational state (STA state)

Interval

The activation cycle (in milliseconds) of the cyclic handler is shown.

Phase

The initial activation phase (in milliseconds) of the cyclic handler is shown.

Time Left

The time left before the next activation (in milliseconds) of the cyclic handler is shown.

Note that if the current state of the cyclic handler is "non-operational state" and the existence of saved activation phases is "no saved", "--" appears.

Start Address

The start address of the cyclic handler is shown.

Extended Information

The extended information of the cyclic handler is shown.

Attribute

The attributes of the cyclic handler (coding language of cyclic handler, initial activation state of cyclic handler and existence of saved activation phases) are shown in the following format.

Coding language Initial activation state Existence

[Coding language of cyclic handler]

TA_HLNG

C language

TA_ASM

Assembly language

[Initial activation state of cyclic handler]

TA_STA

Operational state (STA state)

Nothing displayed

Non-operational state (STP state)

[Existence of saved activation phases]

TA_PHS

There are saved activation phases.

Nothing displayed

There are no saved activation phases.



Remark Double-clicking a cyclic handler information cell (such as Cyclic Handler Name or ID) displays the source file of the cyclic handler in the Editor panel and moves the caret to the relevant location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Cyclic Handler Name, ID, Status, Interval, Phase, Time Left, Start Address, Extended Information, Attribute

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

ID, Interval, Phase, Time Left, Start Address, Extended Information

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Jump to Source (Start Address)

Opens the Editor panel, and displays the source code of the cyclic handler.

Jump to Disassemble (Start Address)

Opens the Disassemble panel, and displays the results of disassembling the cyclic handler.

Service Call

Displays the types of service calls that can be issued.

Note that if a service call is not embedded in (linked to) the downloaded program, or the necessary conditions for executing the service-call process are not met, then the service call will be grayed out.

sta_cyc

Start cyclic handler operation.

stp_cyc

Stop cyclic handler operation.

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).