[Mutex] tab

This tab displays the mutex information (e.g. Mutex Name and ID) of the RI850V4.

Figure A-17. [Mutex] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

(a) First layer

This layer displays the mutex information (e.g. Mutex Name and ID) of the RI850V4.

This layer consists of the following items.

Mutex Name

An icon indicating the current status of the mutex and the name of the mutex are shown in the following format.

Icon Name

Note that if the name of the mutex is undefined, the name will appear as "ID".

The task is locking the mutex (waiting tasks).

The task is locking the mutex (no waiting tasks).

There are no waiting tasks.

ID

The ID of the mutex is shown.

Queue Status

The current status of the mutex is shown.

Waiting Tasks

There are waiting tasks.

Empty

There are no waiting tasks.

Locking Task ID

The ID of the locking task is shown.

Attribute

The task queuing method is shown.

TA_TFIFO

FIFO order

TA_TPRI

Task priority order

Ceiling Priority

"--" is shown.



(b) Second layer

The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the mutex's wait queue.

See the [Task] tab for details about waiting task information.

Figure A-18. [Mutex] Tab (Waiting Task Information)



Remarks 1. Double-clicking a waiting-task information cell (e.g., Object Name or ID) displays the source file of the task in the Editor panel and moves the caret to the relevant location.

2. Double-clicking the waiting-task information cell for Current Task Stack SP or Task Stack Area displays the contents of the task stack in the Memory panel and moves the caret to the relevant location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Muxtex Name, ID, Queue Status, Locking Task ID, Attribute, Ceiling Priority

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

ID, Locking Task ID, Ceiling Priority

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Service Call

Displays the types of service calls that can be issued.

Note that if a service call is not embedded in (linked to) the downloaded program, or the necessary conditions for executing the service-call process are not met, then the service call will be grayed out.

unl_mtx

Unlock mutex.

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).