build.Link.AdditionalOptions


This property sets or refers to the link options for the active project regarding other additional options.

[Specification format]

build.Link.AdditionalOptions = option

[Setting(s)]

Setting

Description

option

Set the additional link options as strings.

[Reference]

Additional link options (strings)

[Detailed description]

-

This property sets or refers to the link options for the active project regarding other additional options.

-

The options set here are added at the end of the link options group.

[Example of use]

>>>build.Link.AdditionalOptions = "-stack -Total_size"      ... Set multiple options
>>>print build.Link.AdditionalOptions
-stack -Total_size
>>>lopt = build.Link.AdditionalOptions + " -map=file.bls"   ... Refer the current setting and add an option
>>>build.Link.AdditionalOptions = lopt
>>>print build.Link.AdditionalOptions
-stack -Total_size -map=file.bls
>>>