| 
 Other Windows... dialog box 
 | 
This dialog box is used to select one of the divide panels shown in the Main window to activate or close.
Figure A.70  | Other Windows... Dialog Box  | 
 
 
The following items are explained here.
[How to open]
-  | From the [Window] menu, select [Other Windows...].  | 
 
Remark  | [Other Windows...] only appears when ten or more divide panels are open.  | 
 
[Description of each area]
(1)  | Select divide panel area  | 
 
Selecting a divide panel switches the target.
[Function buttons]
| 
 | 
 | 
| 
 
Activate 
 | 
 
Activates the divide panel selected in the Select divide panel area, and close this dialog box. 
 | 
| 
 
Close Window(s) 
 | 
 
Closes the divide panel selected in the Select divide panel area, and close this dialog box. 
 | 
| 
 
Close 
 | 
 
Closes this dialog box. 
 |