| 
 Detail Version Information dialog box 
 | 
This dialog box is used to displays detail version information of this product and the present project information.
Figure A.72  | Detail Version Information Dialog Box  | 
 
 
The following items are explained here.
[How to open]
-  | From the [Help] menu, select [Detail Version Information...].  | 
 
-  | Click the [Detail Version Information...] button in the Message dialog box.  | 
 
[Description of each area]
Show the detail version information of this product and the present project information.
The necessary information is as follows.
| 
 | 
 | 
| 
 
System Information 
 | 
 
OS Version 
 | 
 
Windows information 
 | 
| 
 
Language 
 | 
| 
 
.NET Framework Version 
 | 
| 
 
Application Information 
 | 
 
Product Name 
 | 
 
Information of this product 
 | 
| 
 
Package Version 
 | 
| 
 
Version 
 | 
| 
 
Assembly Version 
 | 
| 
 
Sales AreaNote 1 
 | 
| 
 
Product License 
 | 
| 
 
Additional InformationNote 1 
 | 
| 
 
Execution Place 
 | 
| 
 
Memory Usage 
 | 
| 
 
Plug-in InformationNote 2 
 | 
 
Module name 
 | 
 
Each plug-in information for this product in use 
 | 
| 
 
VersionNote 3 
 | 
| 
 
Assembly VersionNote 3 
 | 
| 
 
DLL file nameNote 3 
 | 
| 
 
URLNote 1 
 | 
| 
 
Present Project InformationNote 4 
 | 
 
Main Project Information 
(Subproject Information) 
 | 
 
This shows the absolute path of the project file (the absolute path including the *.mtpj file name for main projects, and the absolute path including the *.mtsp file name for subprojects). 
 | 
| 
 
Microcontroller Information 
 | 
 
The following item to the specified microcontroller information 
-  | Device file name: List of version  |  
  
 | 
| 
 
Build Tool Information 
 | 
 
The following out of the set build tool plug-in informationNote 5 
-  | Version of the build tool plug-in  |  
  
-  | Version of the compiler package to useNote 1  |  
  
 | 
| 
 
Debug Tool Information 
 | 
 
The following out of the set debug tool plug-in information (if the debug tool is not set, hide) 
-  | Connected debug tool name  |  
  
-  | Version of the debug tool plug-in  |  
  
-  | Version of the debug tool control program  |  
  
 | 
| 
 
The Error Information Which OccurredNote 6 
 | 
 
Detailed information on the occurred error information 
 | 
 
Note 1.  | This is not shown when the information does not exist.   | 
 
Note 2.  | The module name of a plug-in not read in has the suffix "(-)" added to the end. 
The module name of a plug-in read in but not functioning has the suffix "(!)" added to the end.  | 
 
Note 3.  | For a plug-in not read in, this is shown as "-".  | 
 
Note 4.  | This is only shown when projects are opened (when there is subproject, line them up).  | 
 
Note 5.  | These are not shown when the project type is a debug-dedicated project.   | 
 
Note 6.  | This is only shown when this dialog box is opened by the [Detail Version Information...] button in Message dialog box.  | 
 
[[Edit] menu (Detail Version Information dialog box-dedicated items)]
| 
 
Copy 
 | 
 
Copies the selected characters in the detail version information area to the clip board. 
 | 
| 
 
Select All 
 | 
 
Selects all the characters in the detail version information area. 
 | 
 
[Context menu]
| 
 
Copy 
 | 
 
Copies the selected characters in the detail version information area to the clip board. 
 | 
| 
 
Select All 
 | 
 
Selects all the characters in the detail version information area. 
 | 
 
[Function buttons]
| 
 | 
 | 
| 
 
Copy All Text 
 | 
 
Copies all the characters displayed in the detail version information area to the clip board. 
 | 
| 
 
OK 
 | 
 
Closes this dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help of this dialog box. 
 |