Renesas Electronics
Build options are set at the project or file level.
-
Project level: See "2.11.1 Set build options at the project level"
File level: See "2.11.2 Set build options at the file level"