2.8 Set Librarian Options

To set options for the link phase, select the Build tool node on the project tree and select the [Librarian Options] tab on the Property panel.

You can set the various librarian options by setting the necessary properties in this tab.

Caution

This tab is not displayed for the application project.