Reads the alarm conditions (weekday, hour, minute).
#include "r_cg_macrodriver.h" #include "r_cg_rtc.h" void R_RTC_Get_AlarmValue ( rtc_alarm_value_t * const alarm_val ); |
See R_RTC_Set_AlarmValue for details about rtc_alarm_value_t (alarm conditions). |
rtc_alarm_value_t * const alarm_val; |
Pointer to structure in which to store the conditions being read |