Sets the counter value (year, month, weekday, day, hour, minute, second) of the real-time clock.
#include "r_cg_macrodriver.h" #include "r_cg_rtc.h" MD_STATUS R_RTC_Set_CounterValue ( rtc_counter_value_t counter_write_val ); |
Below is an example of the structure rtc_counter_value_t (counter value) for the real-time clock. |
If MD_BUSY1 or MD_BUSY2 is returned, it may be because the counter-operation is stopped, or the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger. |