Reads the counter value (year, month, weekday, day, hour, minute, second) of the real-time clock.
#include "r_cg_macrodriver.h" #include "r_cg_rtc.h" MD_STATUS R_RTC_Get_CounterValue ( rtc_counter_value_t * const counter_read_val ); |
rtc_counter_value_t * const counter_read_val; |
Pointer to structure in which to store the counter value being read |
See R_RTC_Set_CounterValue for details about the rtc_counter_value_t counter value. |
If MD_BUSY1 or MD_BUSY2 is returned, it may be because the counter-operation is stopped, or the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger. |