Starts SCI3 data transmission.
Remark 1. | This API function repeats the byte-level SCI3 transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num. |
Remark 2. | R_SCI3m_Start must be called before this API function is called. |
[Syntax]
#include "r_cg_macrodriver.h"
MD_STATUS R_SCI3m_Send ( const uint8_t * tx_buf, uint16_t tx_num );
|
Remark | nは, is the channel numberを意味します。 |
[Argument(s)]
|
|
|
|
|
|
const uint8_t * tx_buf;
|
Pointer to a buffer storing the transmission data
|
|
|
uint16_t tx_num;
|
Total amount of data to send
|
[Return value]
|
|
|
|
MD_OK
|
Normal completion
|
|
MD_ARGERROR
|
Invalid argument specification
|