R_SCI3m_Multiprocessor_Receive


Starts SCI3 data reception by multiprocessor mode.

Remark 1.

This API function performs byte-level SCI3 reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.

Remark 2.

Starts after this API function is called, and R_SCI3m_Start is then challed.

[Syntax]

MD_STATUS R_SCI3m_Multiprocessor_Receive( uint8_t * rx_buf, uint16_t rx_num, uint8_t rx_id);

Remark

m is the channel number.

[Argument(s)]

I/O

Argument(s)

Description

O

uint8_t * const rx_buf;

Pointer to a buffer storing the received data

I

uint16_t rx_num;

Total amount of data to receive

I

uint8_t rx_id;

Reception id

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification