r_sci3m_callback_receiveend


Performs processing in response to the SCI reception interrupt.

Remark

This API function is called as the callback routine of interrupt process r_sci3m_interrupt_receive corresponding to the CSI reception interrupt.

[Syntax]

void    r_sci3m_callback_receiveend ( void );

Remark

m is the channel number.

[Argument(s)]

None.

 

[Return value]

None.