Below is a list of API functions output by the Code Generator for 8-bit timer use.
Table 3.18 8 API Functions: [8-bit timer]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 8-bit timer pulse unit. | |
|
Starts counting by an 8-bit timer. | |
|
Ends counting by an 8-bit timer. | |
|
Performs user-defined initialization relating to the 8-bit timer pulse unit. | |
|
Performs processing in response to the compare match interrupt. | |
|
Performs processing in response to the overflow interrupt. |