Below is a list of API functions output by the Code Generator for clock generation circuit use.
Table 3.2 API Functions: [Clock Generation Circuit]
| API Function Name | Function | 
| Performs initialization required to control the clock generation circuit. | |
| Performs user-defined initialization relating to the clock generation circuit. | |
| Performs processing in response to the osillation stop detection interrupt. | |
| Performs processing in response to the oscillation stop detection NMI. | |
| Sets the clock source. |