Below is a list of API functions output by the Code Generator for LCD controller / driver use.
Table 3.37 API Functions: [LCD controller / driver]
API Function Name |
Function |
Performs initialization necessary to control the LCD controller / driver. | |
Performs user-defined initialization relating to the LCD controller / driver. | |
Sets the LCD controller / driver to display on status. | |
Sets the LCD controller / driver to display off status. | |
Enables operation of internal voltage boost circuit and capacitor split circuit. | |
Disables operation of internal voltage boost circuit and capacitor split circuit. |