Transmit Frame Setting dialog box [Full-spec emulator][E1][E20]


This dialog box is used to make settings related to the transmit frame shown in the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20].

Figure A.56

Transmit Frame Setting Dialog Box

 

This section describes the following.

[How to open]

-

On the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20], select [Add Transmit Frame...] from the context menu.

-

On the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20], select [Edit Transmit Frame...] from the context menu.

[Description of each area]

(1)

Transmit frame setting area

Make settings related to the transmit frame.

(a)

[Use extend format]

The RS-CAN supports both the normal format and extended format for a CAN bus frame.

Select whether to use the extended format for the frame to be transmitted.

(b)

[ID]

Directly enter the ID of a CAN bus frame into the text box as a hexadecimal value.

The range of values that can be input varies depending on the format as shown below.

Format

Settable Range

Normal

0x0 to 0x7FF

Extend

0x0 to 0x1FFFFFFF

(c)

[Remote frame]

The feature of debugging the CAN bus reception procedure supports only debugging of data frames and remote frames of the CAN bus.

Select whether to transmit a remote frame.

If this check box is selected, the frame is assumed to be a remote frame and data cannot be set in the frame.

(d)

[Data size(Bytes)]

Select the size of a data frame of the CAN bus within the range of 0 to 8 bytes.

(e)

[Data]

Directly enter the data to be transmitted in a data frame of the CAN bus into the text box as a hexadecimal value.

The range of the data that can be input is the range up to the size specified in [Data size(Bytes)].

[Function buttons]

Button

Function

OK

Reflects the settings of a transmit frame that were set in this dialog box to the area for making transmit frame settings on the Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20].

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.