Address Offset Settings dialog box


This dialog box is used to set an offset value of the start address in the address area on the Memory panel.

Figure A.32

Address Offset Settings Dialog Box

 

This section describes the following.

[How to open]

-

On the Memory panel, select [View] >> [Address Offset Value Settings...] from the context menu.

[Description of each area]

(1)

[Address Offset Value] area

Directly enter a hexadecimal value as an offset value for the address display.

The settable range depends on the number of bytes of the memory currently being displayed in a line on the Memory panel, as follows:

Settable range: 0x0 - ("Set value of [Size Notation]" x "The number of view columns") -1

Example

When "Set value of [Size Notation]" is 1 byte and "The number of view columns" is 16 columns:

Offset Value

Displayed Content of Address Area

0x0 (default)

0000
0010
0020

0x1

0001
0011
0021

0x2

0002
0012
0022

[Function buttons]

Button

Function

OK

Displays memory addresses with the specified offset value.

Cancel

Cancels the settings and closes this dialog box.

Help

Displays the help for this dialog box.