r_s12adn_groupb_interrupt

Performs processing in response to the group B scan end interrupt.

Remark This function is called to run interrupt processing for the group B scan end interrupt, which is generated when scanning of the analog inputs allocated to group B is completed.

[Syntax]

static void r_s12adn_groupb_interrupt ( void );

Remark n is the unit number.

[Argument(s)]

None.

[Return value]

None.