Below is a list of API functions output by the Code Generator for 12-bit A/D converter use.
Table 3.30 API Functions: [12-Bit A/D Converter]
API Function Name |
Function |
Performs initialization necessary to control the 12-bit A/D converter. | |
Performs user-defined initialization relating to the 12-bit A/D converter. | |
Performs processing in response to the A/D scan end interrupt. | |
Performs processing in response to the group B scan end interrupt. | |
Starts A/D conversion. | |
Ends A/D conversion. | |
Gets the result of conversion. | |
Sets compare level. | |
Performs processing in response to the compare interrupt. |