R_S12ADn_Set_CompareValue

Sets compare level.

[Syntax]

void R_S12ADn_Set_CompareValue ( uint16_t reg_value0, uint16_t reg_value1);

Remark n is the unit number.

[Argument(s)]

I/O

Argument

Description

I

uint16_t reg_value0;

Register value set to the compare revel register 0

I

uint16_t reg_value1;

Register value set to the compare revel register 1

[Return value]

None.