This service call can be called from tasks that belong to Trusted Domain.
This service call deletes the data queue indicated by dtqid.
When there are waiting tasks for the target data queue by using snd_dtq, tsnd_dtq, rcv_dtq or trcv_dtq, this service call cancels the WAITING state of the tasks and returns E_DLT as a return value of the snd_dtq, tsnd_dtq, rcv_dtq or trcv_dtq.