-
trcv_dtq
-
Receive from data queue (with time-out).
ER trcv_dtq (ID dtqid, VP_INT *p_data, TMO tmout);
|
|
|
|
|
|
ID dtqid;
|
ID number of the data queue.
|
|
|
VP_INT *p_data;
|
Data element received from the data queue.
|
|
|
TMO tmout;
|
Specified time-out (in millisecond).
Value: Specified time-out.
|
This service call processes as follows according to the situation of the data queue specified by the parameter
dtqid.
- There is a data in the data queue.
This service call takes out the oldest data from the data queue and stores the data to the area specified by
p_data.
When there is a task in the transmission wait queue, this service call stores the data sent by the task in the top of the transmission wait queue and moves it from the WAITING state (data transmission wait state) to the READY state.
- There is no data in the data queue and there is a task in the transmission wait queue.
This service call stores the data specified by the task in the top of the transmission wait queue to the area specified by
p_data. As a result, the task is unlinked from the transmission wait queue and moves from the WAITING state (data transmission wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
Note, this situation is caused only when the capacity of the data queue is 0.
- There is no data in the data queue and there is no task in the transmission wait queue.
This service call queues the invoking task to the reception wait queue of the target data queue and moves it from the RUNNING state to the WAITING state with time (data reception wait state).
The receiving WAITING state for a data queue is cancelled in the following cases.
Receiving WAITING State for a Data Queue Cancel Operation
|
|
Data was sent to the data queue area as a result of issuing snd_dtq.
|
|
Data was sent to the data queue area as a result of issuing psnd_dtq.
|
|
Data was sent to the data queue area as a result of issuing ipsnd_dtq.
|
|
Data was sent to the data queue area as a result of issuing tsnd_dtq.
|
|
Data was sent to the data queue area as a result of issuing fsnd_dtq.
|
|
Data was sent to the data queue area as a result of issuing ifsnd_dtq.
|
|
Forced release from waiting (accept rel_wai while waiting).
|
|
Forced release from waiting (accept irel_wai while waiting).
|
|
The time specified by tmout has elapsed.
|
|
Forced release from waiting (accept del_dtq while waiting).
|
|
Note 1 Invoking tasks are queued to the reception wait queue of the target data queue in the order of the data reception request.
Note 2
TMO_FEVR is specified for wait time
tmout, processing equivalent to
rcv_dtq will be executed. When
TMO_POL is specified, processing equivalent to
prcv_dtq will be executed.
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the dispatching disabled state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
|
|
|
|
- Stack pointer points out of user stack for invoking task.
- The operand-write access to the area indicated by p_data has not been permitted to the invoking task.
|
|
|
|
- The data queue specified by dtqid does not exist.
|
|
|
|
Forced release from the WAITING state.
|
|
|
|
Polling failure or specified time has elapsed.
|
|
|
|
|