-
tsnd_dtq
-
Send to data queue (with time-out).
ER tsnd_dtq (ID dtqid, VP_INT data, TMO tmout);
|
|
|
|
ID dtqid;
|
ID number of the data queue.
|
|
VP_INT data;
|
Data element to be sent to the data queue.
|
|
TMO tmout;
|
Specified time-out (in millisecond).
Value: Specified time-out.
|
This service call processes as follows according to the situation of the data queue specified by the parameter
dtqid.
- There is a task in the reception wait queue.
This service call transfers the data specified by parameter
data to the task in the top of the reception wait queue. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (data reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
- There is no task neither in the reception wait queue and transmission wait queue and there is available space in the data queue.
This service call stores the data specified by parameter
data to the data queue.
- There is no task neither in the reception wait queue and transmission wait queue and there is no available space in the data queue, or there is a task in the transmission wait queue.
This service call queues the invoking task to the transmission wait queue of the target data queue and moves it from the RUNNING state to the WAITING state with time (data transmission wait state).
The sending WAITING state for a data queue is cancelled in the following cases.
Sending WAITING State for a Data Queue Cancel Operation
|
|
Available space was secured in the data queue area as a result of issuing rcv_dtq.
|
|
Available space was secured in the data queue area as a result of issuing prcv_dtq.
|
|
Available space was secured in the data queue area as a result of issuing iprcv_dtq.
|
|
Available space was secured in the data queue area as a result of issuing trcv_dtq.
|
|
Forced release from waiting (accept rel_wai while waiting).
|
|
Forced release from waiting (accept irel_wai while waiting).
|
|
The data queue is reset as a result of issuing vrst_dtq.
|
|
The time specified by tmout has elapsed.
|
|
Forced release from waiting (accept del_dtq while waiting).
|
|
Note 1 Data is written to the data queue area of the target data queue in the order of the data transmission request.
Note 2 Invoking tasks are queued to the transmission wait queue of the target data queue in the order specified at creating the data queue (FIFO order or current priority order).
Note 3
TMO_FEVR is specified for wait time
tmout, processing equivalent to
snd_dtq will be executed. When
TMO_POL is specified, processing equivalent to
psnd_dtq will be executed.
|
|
|
|
|
|
|
|
|
|
|
|
|
|
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the dispatching disabled state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
|
|
|
- Stack pointer points out of user stack for invoking task.
|
|
|
- The data queue specified by dtqid does not exist.
|
|
|
Forced release from the WAITING state.
|
|
|
Polling failure or specified time has elapsed.
|
|
|
|
|
|
Released from WAITING state by the object reset ( vrst_dtq)
|