Renesas Electronics
ena_tex Outline Enable task exception. C format ER ena_tex (void); Parameter(s) None. Explanation This service call enables task exception handling for the invoking task. Return value Macro Value Description E_OK 0 Normal completion. E_CTX -25 Context error. - This service call was issued from a non-task. - This service call was issued in the CPU locked state. - This service call was issued in the status "PSW.IPL > kernel interrupt mask level". E_MACV -26 Memory access violation. - Stack pointer points out of user stack for invoking task. E_OBJ -41 Object state error. - A task exception handling routine is not defined for the invoking task.
ER ena_tex (void);