Renesas Electronics
19.2.3 Task exception handling functions The following shows the service calls provided by the RI600PX as the task exception handling functions. Table 19-6 Task Exception Handling Functions Service Call Function Useful Range def_tex Define task exception handling routine Task ras_tex Raise task exception Task iras_tex Raise task exception Non-task dis_tex Disable task exception Task ena_tex Enable task exception Task sns_tex Reference task exception disabled state Task, Non-task ref_tex Reference task exception state Task iref_tex Reference task exception state Non-task