Renesas Electronics
sns_tex Outline Reference task exception disabled state. C format BOOL sns_tex (void); Parameter(s) None. Explanation This service call returns TRUE if the task in the RUNNING state is in the task exception disabled state, and otherwise returns FALSE. Table 19-7 shows the details. Table 19-7 Return value of sns_tex Task in the RUNNING state Task exception handling routine for the task in the RUNNING state Task exception disabled state for the task in the RUNNING state Return value Note Exist Defined Enabled state FALSE Disabled state TRUE Not defined Disabled state TRUE When task exception handling routine is not defined, task exception handling is disabled. Not exist - - TRUE Return value Macro Value Description TRUE 1 Normal completion (task exception disabled state). FALSE 0 Normal completion (task exception enabled state). E_CTX -25 Context error. - This service call was issued in the status PSW.IPL > kernel interrupt mask level.
BOOL sns_tex (void);