This option enables the PIC facility.
When this option is specified, the relocation attribute that can be specified in the .cseg or .section directive is changed. |
If a relocation attribute shown below is specified, an error will occur.
When this option is specified: TEXT
When this option is not specified: PCTEXT
This option only controls the relocation attribute that can be specified. The processing for determining whether there is an error in the code for referencing functions is not performed. |