This option enables the PIROD facility.
The PIROD facility is disabled.
When this option is specified, the relocation attribute that can be specified in the .cseg or .section directive is changed. |
If a relocation attribute shown below is specified, an error will occur.
When this option is specified: CONST, ZCONST, or ZCONST23
When this option is not specified: PCCONST16, PCCONST23, or PCCONST32
This option only controls the relocation attribute that can be specified. The processing for determining whether there is an error in the code for referencing constant data is not performed. |