This option enables the PID facility.
When this option is specified, the relocation attribute that can be specified in the .dseg or .section directive is changed. |
If a relocation attribute shown below is specified, an error will occur.
When this option is specified: DATA, ZDATA, ZDATA23, BSS, ZBSS, or ZBSS23
When this option is not specified: SDATA32, SBSS32, EDATA32, or EBSS32
This option only controls the relocation attribute that can be specified. The processing for determining whether there is an error in the code for referencing data is not performed. |