2.9 Save the Project File

The project's settings information is saved to the project file (*.mtpj).

Select the [File] or [Project] menu >> [Save Project].

When there is a change in the project, the message dialog box below will open.

Figure 2.94

Message Dialog Box

 

To continue with the operation, click the [Yes] button on the dialog box.

The project file is overwritten with the current settings information.