Compare match timer (CMT)
Below is a list of API functions output by the Code Generator for compare match timer use.
Table 3.20 API Functions: [Compare Match Timer]
API Function Name |
Function |
Performs initialization necessary to control the compare match timer. | |
Performs user-defined initialization relating to the compare match timer. | |
Performs processing in response to the compare match interrupt (CMIn). | |
Starts counting by a 16-bit timer. | |
Ends counting by a 16-bit timer. |