Everything

Data transfer controller (DTC)

Below is a list of API functions output by the Code Generator for data transfer controller use.

 

Table 3.9   API Functions: [Data Transfer Controller]

API Function Name

Function

R_DTC_Create

Performs initialization necessary to control the data transfer controller.

R_DTC_Create_UserInit

Performs user-defined initialization relating to the data transfer

controller.

R_DTCm_Start

Allows starting of the data transfer controller.

R_DTCm_Stop

Prohibits starting of the data transfer controller.