Everything

Port output enable 3 (POE3)

Below is a list of API functions output by the Code Generator for port output enable 3 use.

 

Table 3.15 API Functions: [Port Output Enable 3]

API Function Name

Function

R_POE3_Create

Performs initialization necessary to control the port output enable 3.

R_POE3_Create_UserInit

Performs user-defined initialization relating to the port output enable 3.

r_poe3_oein_interrupt

Performs processing in response to the output enable interrupt n (OEIn).

R_POE3_Start

Places the MTU's complementary PWM output pins in the high-impedance state.

R_POE3_Stop

Releases the R_POE3_Stop MTU's complementary PWM output pins from the high-impedance state.

R_POE3_Set_HiZ_MTUn

Sets the high-impedance state for the MTUn pins.

R_POE3_Clear_HiZ_MTUn

Clear the high-impedance state for the MTUn pins.

R_POE3_Set_HiZ_GPTn

Sets the high-impedance state for the GPTn pins.

R_POE3_Clear_HiZ_GPTn

Clear the high-impedance state for the GPTn pins.