Everything

r_rspin_callback_error

Performs processing in response to the RSPI error interrupts.

Remark         This API function is called as the r_rspin_error_interrupt callback routine.

 

[Syntax]

static void    r_rspin_callback_error ( uint8_t err_type );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

O

uint8_t err_type;

Source of the RSPI error interrupt (x is undefined)

  xxxx00x1B    : Overrun error detection

  xxxx01x0B    : Mode fault error detection

  xxxx10x0B    : Parity error detection

 

[Return value]

None.