Everything

r_rspin_callback_receiveend

Performs processing in response to the receive buffer full interrupts.

Remark         This API function is called as the r_rspin_receive_interrupt callback routine.

 

[Syntax]

static void    r_rspin_callback_receiveend ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.