Performs processing in response to the receive buffer full interrupts.
Remark This API function is called to run interrupt processing for the receive buffer full interrupt.
[Syntax]
static void r_rspin_receive_interrupt ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.