Everything
2.11.2.1 Changing the form in which values are displayed

The form in which the data in the [Value] area is displayed can be freely changed using the toolbar buttons shown below.

Notation

Shows the following buttons that change the form in which values are displayed.

 

AutoSelect

Displays the value of a selected item (including low-order item) in predetermined notation (default).

Hexadecimal

Displays the value of a selected item (including low-order item) in hexadecimal.

Signed Decimal

Displays the value of a selected item (including low-order item) in signed decimal.

Unsigned Decimal

Displays the value of a selected item (including low-order item) in unsigned decimal.

Octal

Displays the value of a selected item (including low-order item) in octal.

Binary

Displays the value of the selected item (including sub-items) in binary.

ASCII

Displays the character string of a selected item (including low-order item) in ASCII code.

If the subject consists of 2 bytes or more, characters consisting of 1 byte each are displayed one next to another.

Float

Displays the value of the selected item in Float.

Note that when the value is not 4-byte data, displays it in the default notation.

Double

Displays a selected item in Double.

Except for 8-byte data, however, they are displayed in predetermined notation.

 

Adds a hexadecimal equivalent for the displayed value at the end of it, with the equivalent enclosed in parentheses ( ).