Everything
2.3.1 Select color

Select the colors used to distinguish the type of pins whose information is displayed in the Device Top View panel which is opened as described in “2.3 Open Device Top View Panel”.

To select the color to be displayed, click [Device Top View Settings] tab >> [Device top view color setting] in the Property panel and select the color.

Figure 2.3

Select Color

 

Remark

Select the colors to be displayed for the following six types of items.

Device

Selects the display color of the microcontroller.

Device group text

Selects the display color of the device group.

Device part number text

Selects the display color of the device part number.

Macro highligh

Selects the background color of pins selected in the Device List View panel, on the [Pin Function] tab.

Selected pin

Selects the background color of a pin selected in the Device List View panel, on the [Pin Number] tab.

Unused pins

Selects the display color for unused pins (dual-use pins with no use set in the Device List View panel).