Everything
2.13 Display Analysis Information in Chart

You can display the acquired function information and variable information (including the data information for Smart AnalogNote) in a chart.

To display a chart, click the button on the Main window's toolbar to open the Analysis Chart panel.

The following content is graphed in the Analysis Chart panel.

Note

[E1/E2/E2 Lite/E20[RL78]]
This feature is supported only when the selected microcontroller incorporates a Smart Analog IC.

Figure 2.25

Example of Graphs for Analysis Information (Analysis Chart Panel)