Performs processing in response to the DALI reception end interrupt INTSRDLn.
Remark This API function is called as the callback routine of interrupt process r_dalin_interrupt_receive corresponding to the DALI reception end interrupt INTSRDLn (performed when number of received data specified by R_DALIn_Receive argument rx_num has been completed).
[Syntax]
static void r_dalin_callback_receiveend ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.