Everything

R_DALIn_Receive

Starts DALI data reception.

Remark 1.      This API function performs byte-level DALI reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.

Remark 2.      Actual DALI reception starts after this API function is called, and R_DALIn_Start is then called.

 

[Syntax]

#include       “r_cg_macrodriver.h”

MD_STATUS   R_DALIn_Receive ( uint8_t * const rx_buf, uint16_t rx_num );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

O

uint8_t * const rx_buf;

Pointer to a buffer to store the received data

I

uint16_t rx_num;

Total amount of data to receive

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification