Everything
Everything
top
RL78 API Reference
API FUNCITONS
Function Reference
Serial array unit 4
Usage example
Usage example
Please refer to ‘
Usage example in 3.2.30 Serial Array Unit
’ when using this module as UART.
Differences Information
Previous Topic
r_dalin_callback_softwareoverrun
Next Topic
Asynchronous serial interface LIN-UART
Table of Contents
R_DALIn_Create
r_dalin_interrupt_send
r_dalin_interrupt_receive
r_dalin_interrupt_error
R_DALIn_Start
R_DALIn_Stop
R_DALIn_Send
R_DALIn_Receive
r_dalin_callback_sendend
r_dalin_callback_receiveend
r_dalin_callback_error
r_dalin_callback_softwareoverrun
Usage example