Everything

r_fmc_interrupt

Performs processing in response to the end of frequency measurement interrupt INTFM.

Remark         This API function is called as the interrupt process corresponding to the end of frequency measurement interrupt INTFM.

 

[Syntax]

CA78K0R Compiler

__interrupt static void    r_fmc_interrupt ( void );

 

CC-RL Compiler

static void    __near r_fmc_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.