Subsystem clock frequency measurement circuit
Below is a list of API functions output by the Code Generator for subsystem clock frequency measurement circuit use.
Table 3.15 API Functions: [Subsystem Clock Frequency Measurement Circuit]
API Function Name |
Function |
Performs initialization necessary to control the subsystem clock frequency measurement circuit. | |
Performs user-defined initialization relating to the subsystem clock frequency measurement circuit. | |
Performs processing in response to the end of frequency measurement interrupt INTFM. | |
Starts measurement of the frequency that uses the subsystem clock frequency measurement circuit. | |
Ends measurement of the frequency that uses the subsystem clock frequency measurement circuit. | |
Halts the clock supplied to the subsystem clock frequency measurement circuit. |